机器人
人形机器人
末端执行器
视觉
安全防护
移动机器人
第7轴
自动供料
机器人工作站
软件
服务
控制系统
气动
配件

Robots for Industrial Automation

Whether you're automating a single workstation or optimizing an entire production line, the RBTX Marketplace helps you compare robot systems for a wide range of applications. Explore different robot types and find the right automation solution for your manufacturing process.

Which Robot Is Right for Your Application?

Many companies begin their search by looking for a specific robot type. In reality, choosing the right robot starts with the application. Are you loading a CNC machine, handling parts on a conveyor, palletizing products, or automating an assembly process? Once the task is clearly defined, it's much easier to identify the right solution.

The RBTX Marketplace lets you compare robot systems from multiple manufacturers in one place. Instead of being limited to a single ecosystem, you can evaluate different robot types based on your application, process requirements, and production goals.

Whether you're implementing your first automation project or expanding an existing production cell, selecting the right robot always starts with understanding the process.


Types of Robots

Different robot designs are built for different motion profiles. There is no universal robot that fits every application, which is why manufacturers rely on a variety of robot types depending on speed, reach, payload, and workspace requirements.

Robot Type

Typical Applications

Collaborative Robots (Cobots)

Flexible assembly and material handling

Industrial Robots

High-speed production and heavy-duty applications

SCARA Robots

Assembly and precision pick-and-place

Delta Robots

High-speed sorting and picking

Gantry Robots

Large work envelopes and linear motion

Mobile Robots

Internal logistics and material transport

Humanoid Robots

Pilot projects and emerging automation concepts

7-Axis Robots

Applications requiring increased flexibility

Robot Accessories

Expanding or upgrading existing robot systems

Each category provides additional information about its capabilities, strengths, and ideal applications.


Common Robot Applications

Most manufacturers aren't searching for a robot—they're searching for a way to automate a process. That's why your application should always drive the selection.

Typical applications include:

  • Pick and Place

  • Machine tending

  • Assembly

  • Packaging

  • Palletizing

  • Material handling

  • Quality inspection

  • Dispensing and gluing

  • Screwdriving

  • Sorting and part feeding

The right solution depends on factors such as cycle time, payload, part geometry, required accuracy, and available workspace rather than the industry itself.


What Should You Consider Before Choosing a Robot?

Choosing a robot involves more than comparing technical specifications. Asking the right questions early in the planning phase helps narrow down the available options.

Question

Why It Matters

What parts will the robot handle?

Size, weight, and geometry determine payload and reach requirements.

How fast does the process need to run?

Cycle time influences robot speed and performance.

How much accuracy is required?

Different applications require different levels of repeatability.

How much floor space is available?

Workspace constraints affect robot selection.

Will the application grow over time?

Scalable systems make future expansion easier.

Does the robot need to interact with operators?

The application determines whether collaborative or traditional solutions are more appropriate.

Defining these requirements before selecting hardware makes it easier to identify the right automation solution for your production environment.

When Does Robot Automation Make Sense?

Every automation project starts with a business challenge. For some manufacturers, it's increasing production capacity. For others, it's labor shortages, repetitive manual work, inconsistent quality, or growing demand.

Robots are particularly effective when repetitive tasks need to be performed consistently, accurately, and over long production runs. They can help manufacturers improve process stability, reduce manual handling, and create more efficient production workflows.

Today, robot automation is no longer limited to large-scale manufacturing. Companies of all sizes are using automation to improve productivity while remaining flexible enough to adapt to changing production requirements.


Automation for Manufacturers of All Sizes

Industrial automation has become far more accessible than it was just a few years ago. Many companies begin with a single workstation or production process before expanding automation across additional operations.

For smaller manufacturers, this reduces the barrier to entry and allows automation projects to grow alongside the business. Larger manufacturers benefit from the same flexibility by expanding production capacity, introducing new products, or optimizing existing workflows without redesigning entire production lines.

Regardless of company size, the goal remains the same: selecting the right solution for the application.


Open Automation Gives You More Flexibility

Automation projects rarely remain static. Product designs evolve, production volumes change, and new requirements emerge over time.

Rather than locking manufacturers into a single ecosystem, the RBTX Marketplace follows an open approach. Robot systems can be combined with compatible automation components based on the needs of each application, making it easier to compare solutions and build systems that can adapt as production requirements change.

This flexibility allows manufacturers to scale automation at their own pace while maintaining greater freedom when selecting components for future projects.


Why Different Robot Types Exist

Every robot is designed to solve a different type of motion challenge. Some applications require high speed, while others prioritize precision, payload capacity, reach, or flexibility.

That's why there is no universal robot for every manufacturing process. Selecting the right robot always depends on the specific application rather than simply choosing the most advanced or most powerful system.

Our robot categories provide a starting point for comparing different robot types and understanding which solutions are best suited for your production requirements.


Frequently Asked Questions

Which robot is best for my application?

There is no one-size-fits-all solution. The best robot depends on factors such as payload, reach, cycle time, accuracy, workspace, and the specific manufacturing process you want to automate.

Can small manufacturers benefit from robot automation?

Yes. Many companies begin by automating a single task before expanding automation to additional processes. This approach helps reduce investment risk while providing immediate operational benefits.

What applications can robots automate?

Robot systems are commonly used for pick and place, machine tending, assembly, packaging, palletizing, material handling, quality inspection, dispensing, screwdriving, and many other repetitive manufacturing tasks.

What's the difference between collaborative and industrial robots?

Collaborative robots and traditional industrial robots are designed for different applications. The right choice depends on factors such as payload, speed, workspace, tooling, and the results of a risk assessment.

Can a robot system be expanded later?

Many automation projects evolve over time. Depending on the application, robot systems can often be expanded or adapted as production requirements change.


Find the Right Robot for Your Automation Project

Whether you're planning your first automation project or expanding an existing production line, the RBTX Marketplace helps you compare robot systems for a wide range of manufacturing applications. Browse our robot categories to explore different solutions and find the right technology for your production goals.