Study - Rotation conveyor
产品代码: 0-RBTX-BASICS-0039
多种规格: Ø280mm
The rotary conveyor developed by Igus is used for feeding, positioning and separating small components. These can be picked by robot kinematics or fed to a production line. A rotating felt disc jerks the inserted components into motion, causing them to change their position spontaneously.
The operator determines which parts he wants to convey and is also responsible for fitting the attachments (baffles etc.) that are required for conveying and further processing certain desired small parts. These attachments can be fastened to the screw connections of the modular limit.
一般交货时间:3周
单独购买,只需清空您的“完整方案配置器”
亮点
投资回报快
供料系统的投资成本往往很高,而且摊销速度很慢。
使用这款低成本的旋转式输送机,您可以在短时间内实现投资回报。
使用RBTX构建低成本的解决方案
与我们的RBTXpert预约免费视频通话
选择您合适的时段
向我们展示您的应用
igus专家与您一起寻找所有组件
您将获得固定价格的报价