机器人
人形机器人
末端执行器
视觉
安全防护
移动机器人
第7轴
自动供料
机器人工作站
软件
服务
控制系统
气动
配件

Robot Pneumatics

Robot pneumatics use compressed air or vacuum to grip, lift, move, clamp or dispense materials. On RBTX, you can compare compact ejectors, valves, control boxes and vacuum pumps . The right choice depends on your workpiece, cycle time, robot and end effector.

What Are Robot Pneumatics?

In pneumatic robotics, compressed air is used to create movement or generate vacuum. This allows a robot to pick up, hold, move and release a workpiece.

A robotic pneumatic system may include:

  • Pneumatic grippers

  • Vacuum ejectors

  • Vacuum pumps

  • Valves

  • Tubing and fittings

  • Pressure or vacuum sensors

  • Control boxes

  • Pneumatic actuators

The required components depend on the application. A smooth metal sheet needs a different gripping solution than a porous cardboard box, a fragile food product or a heavy machined part.

Which Pneumatic Solution Fits Your Application?

The following table provides a first point of reference.

Task

Typical solution

Important selection criteria

Pick up smooth parts

Vacuum ejector or vacuum pump with suction cups

Surface, weight and cup size

Grip parts from the outside

Pneumatic parallel gripper

Gripping force, stroke and part shape

Handle sensitive products

Soft gripper or flexible end effector

Material, pressure and permitted contact force

Clamp a component

Pneumatic gripper or cylinder

Holding force, position and safety

Push or move a part

Pneumatic actuator

Stroke, speed and available space

Operate without compressed air

Electric vacuum pump or electric gripper

Power supply, weight and control

Pneumatic and electric grippers have different strengths. Pneumatic grippers are often suitable for simple, fast open-and-close movements. Electric grippers can be useful when the gripping position or force needs to be adjusted for different parts.

Pneumatic Gripper or Vacuum Gripper?

These are two common options for robot handling.

Pneumatic grippers

A pneumatic gripper uses jaws or fingers to hold a part. It is often suitable for solid components with accessible and repeatable gripping points.

Common applications include:

  • Machine tending

  • Assembly

  • Sorting

  • Pick and place

  • Part removal

The main selection criteria are gripping force, jaw stroke, part shape and finger design.

Vacuum grippers

A vacuum gripper holds a workpiece using suction. It is often suitable for flat, smooth or sensitive surfaces.

Typical workpieces include:

  • Sheet metal

  • Plastic parts

  • Glass

  • Packaging

  • Boxes

  • Panels

Air can leak through porous, rough or uneven surfaces. In these applications, the vacuum generator must provide enough flow to maintain a reliable grip.

Ejector or Vacuum Pump?

A pneumatic ejector generates vacuum using compressed air. An electric vacuum pump generates vacuum using electrical power.

Solution

Usually suitable when…

Check before selecting

Pneumatic ejector

Compressed air is already available

Air consumption, tubing length and valves

Compact ejector

Vacuum should be generated close to the gripper

Connection, suction capacity and control

Electric vacuum pump

No central compressed-air supply is available

Weight, power supply and installation space

Central vacuum supply

Several suction cups or stations need vacuum

Tubing distances, pressure losses and control

A larger vacuum generator is not automatically the better choice. It must create and maintain enough vacuum for the workpiece while meeting the required gripping time.

Vacuum systems can include suction cups, generators, filters, sensors and regulators. Pneumatic systems may also require directional valves, air preparation equipment, fittings and tubing.

Five Important Selection Criteria

1. Workpiece

Start by checking:

  • Weight

  • Size

  • Shape

  • Surface

  • Material

  • Center of gravity

  • Sensitivity

A smooth plastic component is usually easier to pick up with vacuum than a porous box. A delicate product may require a softer contact surface or lower gripping force than a robust metal part.

2. Robot motion and cycle time

The end effector must hold the part during acceleration, braking and changes in direction. The workpiece weight alone is therefore not enough to select the system.

Check:

  • How fast does the robot move?

  • Will the workpiece be rotated?

  • Will it be moved overhead?

  • How quickly must it be gripped and released?

Shorter cycle times may require faster valves, shorter tubing and a suitable vacuum flow rate.

3. Robot payload

The robot carries more than the workpiece. Include the weight of:

  • Gripper or suction cups

  • Valves

  • Sensors

  • Adapter plate

  • Tubing

  • Tool changer

  • Workpiece

The complete load, its center of gravity and the resulting moments must stay within the robot manufacturer’s limits.

4. Compressed-air supply

Before selecting industrial robot pneumatics, check:

  • Is compressed air available at the workstation?

  • What operating pressure is available?

  • Is the available air flow sufficient?

  • How long will the tubing be?

  • Can the ejector or valve be installed close to the gripper?

Long or undersized tubing can slow down the response of the system.

5. Robot control and sensors

The robot controller or PLC must be able to operate the valve, pump or control box.

Check:

  • Supply voltage

  • Digital inputs and outputs

  • Communication interfaces

  • Sensor connections

  • Feedback signals

A pressure or vacuum sensor can confirm that a part has been picked up before the robot continues its movement.

Application Matrix for Pneumatic Automation

Application

Typical pneumatic solution

Important factors

Pick and place

Vacuum gripper or pneumatic gripper

Cycle time, weight and surface

Machine tending

Parallel gripper or vacuum gripper

Chips, coolant and part detection

Packaging

Vacuum gripper or soft gripper

Sensitive products and changing shapes

Palletizing

Multiple suction cups or area gripper

Box surface, payload and air leakage

Assembly

Pneumatic gripper or cylinder

Position, force and tolerances

Sorting

Suction cup, gripper or flexible end effector

Different part sizes and shapes

Dispensing and gluing

Pneumatic dispensing components

Material, pressure and dispensing volume

Laboratory automation

Small gripper or suction cup

Cleanliness, repeatability and fragile containers

Pneumatic actuators are available for linear, guided, rotary, clamping and pick-and-place tasks. This makes them suitable for more than gripping alone.

What Additional Components Are Required?

A pneumatic gripper or vacuum cup is usually only one part of the complete system.

Depending on the application, you may also need:

  • Directional valves

  • Tubing and fittings

  • Pressure regulators

  • Filters

  • Sensors

  • Adapter plates

  • Custom gripper fingers

  • Suction cups

  • Control boxes

  • Vacuum generators

  • Check valves

Before ordering, check which components are included with the product and which must be purchased separately.

Safety for Pneumatic End Effectors

A cobot does not automatically make a pneumatic application safe.

The complete application must be considered, including:

  • Robot

  • End effector

  • Workpiece

  • Speed

  • Work area

  • Pinch and crushing points

  • Risk of dropping the part

It is especially important to define what happens during a loss of air pressure, electrical power or control signal.

Depending on the application and risk assessment, additional measures may include:

  • Vacuum monitoring

  • Check valves

  • Mechanical retention

  • Controlled part placement

  • Guards or enclosures

  • Safely limited speed

The required protective measures depend on the complete robot application, not only on the gripper.

Quick Selection Guide for Robot Pneumatics

Question

Why it matters

What needs to be handled?

Determines the gripper type and contact surface

How heavy is the workpiece?

Affects gripping force and vacuum capacity

Is the surface smooth or porous?

Important for vacuum gripping

How fast must the robot operate?

Affects valves, flow and gripping time

Is compressed air available?

Helps determine whether a pneumatic or electric solution is suitable

Which signals can the controller process?

Important for valves, pumps and sensors

What happens if power or pressure is lost?

Important for safe part retention

Will different parts be handled?

Affects stroke, finger design and flexibility

Frequently Asked Questions About Robot Pneumatics

What are robot pneumatics?

Robot pneumatics are components that use compressed air or vacuum for gripping, clamping, lifting or moving tasks in robotic automation.

What are pneumatic grippers used for?

Pneumatic grippers are commonly used for pick and place, assembly, machine tending, sorting and part removal.

When should I use a vacuum gripper?

A vacuum gripper is often suitable for flat, smooth or sensitive workpieces such as sheet metal, glass, plastic parts and packaging.

Do all pneumatic grippers require compressed air?

Yes. Pneumatic grippers and pneumatic ejectors need a suitable compressed-air supply. An electric gripper or electric vacuum pump may be an alternative when compressed air is not available.

What is the difference between an ejector and a vacuum pump?

An ejector generates vacuum using compressed air. An electric vacuum pump uses electrical power.

Can one gripper handle different workpieces?

It may be possible when the gripper stroke, finger design and gripping force cover the full range of parts. Larger differences may require interchangeable fingers, a flexible gripper or a tool changer.

How can the robot detect a successful grip?

Pressure sensors, vacuum sensors or position switches can provide a feedback signal to the robot controller or PLC.

What happens if the air pressure drops?

That depends on the system design. The workpiece may be released if no retention measure is provided. Pressure loss and power failure should therefore be considered during planning and risk assessment.

Which pneumatic components fit my robot?

Compatibility depends on the robot flange, payload, controller, available connections, end-effector weight and application. The complete tool load and center of gravity must also be checked.

Check Your Pneumatic Solution Before Purchase

Not sure which gripper, ejector, valve, sensor or vacuum pump fits your application? RBTX helps you compare components and plan the complete setup.

Book a free expert video call

Discuss your workpiece, robot, cycle time and available compressed-air supply with an RBTXpert.

Test the application before investing

A feasibility test can help determine whether the workpiece can be gripped, moved and released reliably. RBTX lists expert video calls and feasibility tests among its available services.

Request a turnkey automation solution

When individual components are not enough, RBTX can also support the planning and integration of a complete automation solution.

Next step: Compare robot pneumatics, request a feasibility test or book a free RBTXpert consultation.