机器人
人形机器人
末端执行器
视觉
安全防护
移动机器人
第7轴
自动供料
机器人工作站
软件
服务
控制系统
气动
配件

Robot Accessories:

The right robot accessories turn a robot into a complete automation solution. Adapter plates connect the robot to its tooling, energy chains guide cables and hoses, mounting systems provide a stable base, and sensors help detect workpieces or process states.

Robot Accessories for Different Automation Tasks

Not every technical detail needs to be defined at the start. The first step is to identify the function the accessory should perform.

Automation task

Common accessories

Mount and position the robot

Base, mounting plate or frame

Connect a gripper or process tool

Adapter plate or flange adapter

Guide cables and hoses

Energy chain, protective conduit or cable holder

Use several tools on one robot

Manual or automatic tool changer

Set up and operate the robot

Teach pendant or handheld controller

Detect workpieces

Sensor, photoelectric sensor or light barrier

Measure process forces

Force-torque sensor

Improve camera images

Machine or vision lighting

Extend the working range

External axis or rotary axis

Protect the robot from contamination

Robot cover

A basic pick-and-place application may only require a stable mounting solution, a suitable gripper adapter and cable guidance. More advanced systems may also need sensors, lighting, automatic tool changing or an additional axis.

When the required robot components are not yet clear, RBTX can consider the complete setup and help select individual products or plan a turnkey automation solution.

What Is Included in Robot Accessories?

Robotic accessories are components that connect, extend, protect or support a robot application.

Common product groups include:

  • Adapter and mounting plates

  • Robot bases and frames

  • Energy chains and cable holders

  • Tool changers

  • Teach pendants and handheld controllers

  • Force-torque sensors

  • Photoelectric and proximity sensors

  • Machine and vision lighting

  • Protective covers

  • External axes

  • Cables, hoses and mounting brackets

  • Equipment for mobile robot systems

The line between accessories, peripheral equipment and other automation components is not always fixed. What matters most is the function of the product within the application. The current RBTX selection includes products such as adapter plates, energy chain systems, sensors, external axes, lighting and operating devices.

Main Types of Robot Accessories Explained

Adapter Plates and Flange Adapters

An adapter plate connects the robot to a gripper, sensor or process tool. It is required when the two components cannot be mounted directly together.

The following information is usually enough for an initial selection:

  • Robot manufacturer and model

  • Gripper or tool manufacturer and model

  • Intended application

  • Required electrical, signal or pneumatic connections

Measuring the flange pattern is usually not necessary at the beginning. Existing product data can be used to determine whether a standard adapter is available or whether another solution is needed.

Robot Bases and Mounting Systems

A robot base or mounting plate provides a stable installation and positions the robot at a suitable working height.

Useful information for the first selection includes:

  • Robot model

  • Floor, table, frame or mobile installation

  • Approximate working area

  • Available installation space

  • Environmental conditions such as chips, moisture or frequent relocation

This information helps narrow down the mounting solution. For a complete system, the robot position can also be considered together with the required reach and surrounding equipment.

Energy Chains and Cable Management

Cables and hoses move whenever the robot moves. Suitable cable management prevents them from hanging loosely in the workspace, rubbing against equipment or becoming trapped.

Common solutions include:

  • Energy chains

  • Protective conduits

  • Cable clips

  • Mounting brackets

  • Guide systems

  • Complete cable kits

Robot model, tooling and required lines are the most important starting points. The exact cable route does not need to be fully planned in advance. For a turnkey system, cable and hose guidance can be coordinated with the robot, end effector and motion sequence.

Tool Changers

A tool changer allows one robot to use different grippers or process tools.

Type

Typical use

Manual tool changer

Tools are changed occasionally by personnel

Automatic tool changer

The robot changes tools during the process

Mechanical connection only

No electrical or pneumatic transfer is required

Tool changer with media transfer

Power, signals or compressed air are transferred

For an initial assessment, it is helpful to know which tools will be used and how often they need to be changed. Additional requirements such as tool stands and media connections can then be included in the system design.

Teach Pendants and Handheld Controllers

A teach pendant is used to set up and operate a robot. Depending on the device, it may support functions such as moving the robot, teaching positions, selecting programs or starting processes.

Teach pendants are normally designed for specific robot controllers. The robot and controller models are therefore the most important information for selecting a suitable device.

Sensors

Sensors provide information about workpieces, positions and process conditions.

Typical tasks include:

  • Detecting the presence of a part

  • Checking a position

  • Measuring distance

  • Confirming a gripping process

  • Measuring forces at the tool

A force-torque sensor can capture forces and moments acting at the robot tool. This can be useful in assembly, joining and inspection processes.

For the initial selection, a short description of what needs to be detected or measured is usually sufficient. The suitable sensor type can then be chosen based on the object, distance and installation situation.

Machine and Vision Lighting

Cameras need suitable lighting to detect components and inspection features reliably. Machine lights can also improve visibility inside the robot workspace.

Helpful information includes:

  • The workpiece or feature to be detected

  • Part size and surface

  • Camera type

  • Available installation space

  • Possible reflections or shadows

Lighting should be selected together with the camera and inspection task. The shape, angle and type of light can strongly affect the image result.

Protective Robot Covers

A cover can help protect a robot from dust, dirt or other environmental influences.

The cover should:

  • Fit the robot model

  • Allow the required movements

  • Suit the working environment

  • Keep necessary connections accessible

Robot model and environmental conditions are usually enough to identify suitable options for an initial comparison.

External Axes

An external axis adds another movement to the robot system. It can move either the robot or the workpiece.

Typical versions include:

  • Linear axes

  • Travel axes

  • Rotary axes

  • Positioners

External axes are used when the robot needs to reach several stations or when a workpiece must be rotated during the process. The RBTX range includes external rotary axes and energy chain solutions for multi-axis robot systems.

A detailed technical specification is not required for the first inquiry. Information about the robot, workpiece and desired movement usually provides a suitable starting point.

Application Matrix for Industrial Robot Accessories

Application

Common robot accessories

Main purpose

Pick and place

Adapter plate, cable holder, sensor

Mount tooling and detect parts

Machine tending

Robot base, protective conduit, sensors

Position the robot and protect lines

Palletizing

Mounting base, energy chain, external axis

Support reach and cable guidance

Assembly

Adapter plate, force sensor, tool changer

Connect tools and monitor process forces

Quality inspection

Lighting, sensors, camera mounts

Produce stable images and repeatable inspections

Welding or dispensing

Cable management, tool holder, positioner

Guide lines and orient workpieces

Changing production tasks

Tool changer and tool station

Use several tools with one robot

Mobile automation

Mobile base, mounting hardware, charging equipment

Move the system between work areas

Education and training

Mounting kit, operating device, protective equipment

Create a complete training setup

Information That Helps Narrow Down the Selection

A complete technical plan is not required before choosing accessories. Four basic pieces of information are often enough for a first assessment.

1. Robot Model

The manufacturer and model help identify compatible adapter plates, bases, cable kits and operating devices.

2. Intended Application

A brief process description can be sufficient, for example:

  • Pick up and place components

  • Load and unload a machine

  • Palletize boxes

  • Inspect parts

  • Change tools automatically

This indicates which accessory groups are likely to be relevant.

3. Tooling

When already known, the planned gripper, suction system, sensor, camera or process tool should be included. When tooling has not yet been selected, it can be considered together with the required accessories.

4. Working Environment

Useful details include available space, mounting location and environmental conditions. A sketch, photo or short video can often provide enough context for an initial discussion.

Missing information can be clarified during the next planning step. For turnkey systems, RBTX can include the required accessories directly in the overall concept.

Robot Accessories, Components and Spare Parts

Term

Meaning

Robot accessories

Products that extend or support an application

Robot components

Individual building blocks of the automation system

Robot peripheral equipment

Devices and systems around the robot

Robot spare parts

Products intended to replace worn or damaged parts

An adapter plate is a typical robot accessory. A sensor or gripper is a component of the application. A replacement cable for a specific robot may instead be a spare part.

For robot replacement parts, the exact product identification of the existing part is important. A product with a similar appearance is not automatically a suitable replacement. Robot-parts catalogs can cover very different products, from wiring and sensors to actuators and mechanical components, so the required system and purpose should be identified clearly.

Frequently Asked Questions About Robot Accessories

What products are considered robot accessories?

Common examples include adapter plates, robot bases, energy chains, cable holders, tool changers, teach pendants, sensors, lighting, protective covers and external axes.

Which accessories are typically needed for a first robot application?

Many basic applications require stable mounting, a connection between the robot and end effector, and suitable cable or hose guidance. Additional products depend on the task and working environment.

Do all technical dimensions need to be known before ordering?

No. Robot model, tooling and a short application description are often enough for an initial selection. Additional details can be clarified during the planning process.

Does every accessory fit every robot?

No. Accessories may be designed for specific robots, controllers or tools. The manufacturer and exact model should therefore be considered.

When is an adapter plate required?

An adapter plate is required when the robot flange and tool cannot be connected directly.

When is a tool changer useful?

A tool changer is useful when the same robot needs to operate several grippers or process tools.

Why is cable management important?

Suitable cable management protects cables and hoses and prevents them from interfering with the robot movement or workspace.

Can accessories be included in the complete system planning?

Yes. When the required products have not yet been defined, RBTX can review the application and include suitable accessories in the system concept.

Are complete automation solutions also available?

In addition to individual products, RBTX can support the planning and implementation of a turnkey automation solution. The robot, tooling, accessories, control system and other required components can be considered together. RBTX also offers expert video calls and feasibility testing as part of its service options.

Select Compatible Robot Accessories

When the required adapter plate, mounting solution, energy chain or sensor system is still open, RBTX can support the selection and combination of suitable products.

Book a free expert video call

During a free 30-minute RBTXpert video call, the robot model, application and open accessory questions can be reviewed together.

Test the application before purchasing

A feasibility test can help determine whether the robot, tooling, accessories and workpiece operate together as planned.

Request a turnkey automation solution

For a complete automation project, RBTX can include the necessary accessories from the start—from mounting and adapter plates to cable management, sensors and integration.

Next step: Compare robot accessories, book a free consultation or request a complete automation solution.